I'm working on a high capacity pack, and the theoretical capacity is greater than the maximum design capacity that can be set in the dataflash.
How big of a problem is this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm working on a high capacity pack, and the theoretical capacity is greater than the maximum design capacity that can be set in the dataflash.
How big of a problem is this?
Hi Greg,
This should not be a problem. This document should be helpful:
By the way, I recommend using the BQ78350-R1A which comes pre-loaded with the latest firmware. It is identical to the BQ78350-R1 except there was an improvement to the firmware to make the Shutdown feature more robust.
Best regards,
Matt
I have some questions on the current scaling for high capacity packs.
Page 5 says to scale all current and capacity flash values except AOCD, ASCC and ASCD. Why wouldn't I scale those to be in line with the scaled calibration?
Never mind. Those parameters are voltage based, not current based.
On page 26 of the slide deck, there are two parameters under "not scaled" and six parameters that are in boxes. Which of those are scaled and which ones are not? This seems to contradict page 5.
Hi Greg,
All of the units in mA and mAh need to be scaled. This was a from a live presentation, so I'm not sure what the significance of the boxes is.