Hi team,
If we would like BQ76942 alert pin to set high when discharge current reaches 50mV so we could use the alert pin signal to awake the MCU.
How to do the configuration? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
If we would like BQ76942 alert pin to set high when discharge current reaches 50mV so we could use the alert pin signal to awake the MCU.
How to do the configuration? Thanks!
Hi Brian,
I'm not sure I understand: do you mean 50 mA for the discharge current?
For this behavior, you can set the following settings:
When the device exits Sleep mode, the ALERT pin will go high with these settings. Then, you need to write 0x0001 to the Alarm Status register (0x62) to clear the WAKE bit to reset the ALERT pin.
Best regards,
Matt
Hi Matt,
Sorry I had just noticed the reply.
The understanding is slightly different from what we meant.
Customer are trying to use the alert pin to awake MCU even when AFE is awake. So we prefer to use 50mV OCD to pull up the alert pin rather than sleep event.
Please also note customer do not what any protection actions when this 50mV OCD happens since it is only used to alert the MCU. Is it possible to do so?
Regards,
Brian
Hi Brian,
You can set the DSG FET Protections A register to 0x80. This will configure the DSG FET to only disable in the case of a SCD and not for OCD.
Regards,
Matt