This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089: Output capacitor

Part Number: TPS61089

Hi team,

My customer is considering the TPS61089. Currently, the customer is using ceramic cap for output, but the load change is large, they would like to add electrolytic cap to increase the capacitance.  Is it OK to add an electrolytic capacitor in parallel with a ceramic capacitor if the phase compensation is done properly? 

The d/s explains the Loop Stability calculation, but it is complicated, so if you have execl calculation sheet, could you send me it?

Vin=3.6V,

Vout=11.2V,

Iout=1-2A,

Regards,

Yamaguchi