This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515-Q1: IR LED

Part Number: TPS92515-Q1


Hello

IR LED current is set to 800mA.

During the test in 85 degree environment, the IR LED turns on and off. (3 second cycle)

Is there a protection function related to temperature?

If so, at what temperature will it operate and at what temperature will it be released?

Or is there another reason?

The temperature inside is over 100 degrees.

Please help me.