This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62812-Q1: Low side Current limit

Part Number: TPS62812-Q1

Hi team,

Could you advise the low side current limit value described in the datasheet P17 9.4.4 as below?

I could not find the spec in EC table. 

"The high-side switch turns on again only if the current in the low-side switch has decreased
below the low-side current limit."

regards,

  • Hi Shinji,

    TPS6281x-Q1 device has similar high side and low side FET according to their current variant. The current limit is same for HSFET and LSFET. TPS62812-Q1 is min 2.8A and Max 4.2A.

    Best regards,

    Tanvee

  • Hi Tanvee,

    Do you mean HS and LS current limit is almost same and the average clamp current at current limit is ILIMH?

    Could you also advise the tolerance of the 50ns propagation delay to calculate the Ipeak?

    regards,

  • Hi Tanvee,

    Could you also advise how does the device behaves when the out put hard short to GND?

    regards,

  • Hi Shinji,

    We didn't define tol. for propagation delay. you can use the typical value (50ns) for calculation.

    Normally during short inductor current have high peak goes outside current limit and it will turn on LS to make it inside current limit. you can find detail description in section 9.4.4 in the datasheet.

    Best regards,

    Tanvee

  • Hi Tanvee, 

    Could you advise if my understanding below is correct?

    If Vout is short to GND, then the current is clamped to ILIMH + (Ipeak - ILIMH)/2. 

    regards,

  • Hi Shinji,

    Yes, it is correct the peak current statics value can be evaluated through this equation.

    Best regards,

    Tanvee