Other Parts Discussed in Thread: TPS25750
Hello everyone,
I'm writing this post as a follow-up to https://e2e.ti.com/support/power-management/f/196/t/967957 this, where I was guided to use TPS25750D for my USB-C Power Delivery. Now I have some questions and I want to validate my design for my university project.
I want my device to operate with the following conditions:
Input voltage 15V negotiated by USB-C
Input current 3A (I guess 45W is all I can get with 15V input)
Output Voltage: 5V, converted by the switching circuit.
Output current 8A max
I came up with this schematic:
The questions I have are:
a) How will my USB C PD chip TPS25750D determine what voltage to select and then negotiate through USB-C? I understand that the resistors
b) I have 6 peripheral devices. How can I isolate the 6 terminals (bottom right of the schematic) such that my devices don't interfere with each other (i.e if 3-4 devices are stopped at the same time/start at the same time, there could be a load change in the circuit and before the buck converter responds, I might get spikes/fluctuations)? Each will use a maximum of 5V 1.5A. It's possible all 6 are connected or only one is connected at a time.
Thank you for your time and I'm looking forward to your answer.