This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54620: About TPS54620 P2P replace TPS54320

Part Number: TPS54620
Other Parts Discussed in Thread: TPS54320,

Hi team,

My customer use our TPS54320, but TPS54320 have a tight supply, so they want to use TPS54620 which is P2P with TPS54320 to replace TPS54320.

I see just the load capacity and the internal switching frequency are different between TPS54320 and TPS54620, and our customer use three TPS54320 for 12V to 1.8V/3.3V/1.2V,the attachment is the schematic of three application.

Whether the peripheral parameters, especially the loop compensation parameters, can be directly replaced from tps54320 to TPS54620 under the existing BOM, please help me check it thanks.

It is our supply problem that caused the customer to have to replace it, please help to deal with it as soon as possible, thank you very much.

About TPS54620 P2P replace TPS54320.pptx

Best regards,

Andy