This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156-Q1: recommend device

Part Number: LM5156-Q1
Other Parts Discussed in Thread: LM5176, LM5118

Hi Sirs,

My customer is looking for a buck-boost device that can output 140W and pass the ISO16750-2 standard. (Vin_min is 3.5V, Vin_max is 60V; V-out is 14V; I-out is 10A)

May I know the LM5156-Q1 can meet their request? or advise other devices. Thanks!