Hi, I want to use TPS65400 for a very small design where I need 0.72/0.85V@4A, 1.8V@4A, 3.3V@2A and 5.0V@2A using 9-15VVIN (battery).
Webench errors on 0.85V. Why? I want to make sure this simulates before I buy EVM and proceed. - Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I want to use TPS65400 for a very small design where I need 0.72/0.85V@4A, 1.8V@4A, 3.3V@2A and 5.0V@2A using 9-15VVIN (battery).
Webench errors on 0.85V. Why? I want to make sure this simulates before I buy EVM and proceed. - Patrick
Hi Patrick
There is no problem for your design, but the frequency in Webench is fixed to 500kHz, so it cannot update the design. If you want to check your design, you can use pspice and also you can refer to the user guide of TPS65400. Thanks.
BR
Ruby