Hello Support team,
TPS53515 has output discharge circuit.
According to datasheet, IVODIS is defined as 10~15mA at VVO=0.5V condition.
Does it mean that discharge current depends on the output voltage condition?
Will the internal discharge resistance discharge output capacitance?
If it is true, please let me know the min / typ / max of discharge resistance.
Can the discharge function continues to work until Vout=0V?
If there are the disable condition, please let me know.
Could you please let me know any formula to calculate the shutdown time after EN disable?
Best Regards,
Hirokazu Takahashi