This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Our customer would like to request a schematic design review of BQ24072 and BQ27520-G4. Here is the schematic diagram.
Thank you for your support!
Regards,
Danilo
Hi Danilo,
Upon review of the schematic everything on the BQ24072 looks okay, although the customer mentions on the schematic they want to ISET = 863 mA, but R14 connected to ISET is 3K. To set ISET = 863 mA R14 should be 1.03 Kohms.
There are a few things which need adjustment on the BQ27520-G4. A ground connection should be added between C13 and C17. The SRP pin needs to be connected to the battery pack (-) terminal (labeled LiIon- on customer schematic) and SRN needs to be connected to ground instead of battery pack-.
Regards,
Garrett
Hi Garret,
Thank you very much for your valuable feedback. I have updated the customer and still waiting for his response if he needs further assistance.
Regards,
Danilo