This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Based on the error message you provided, there are two general categories of potential problems:
1. Electrical problems: missing / unsuitable pull-up resistors for bus length
2. Address problems: mismatched slave address or not-ready ACK state
Regarding the problems, there are multiple ways to check:
1. Please verify the schematic with our customer and send me a copy of that
2. Please also send me waveforms of I2C communication
3. Test if this problem prevail to other devices (not just LP5036)
4. Refer to the previous e2e thread on this topic (hyperlinked): LP5036 I2C NACK
Best Regards,
Aaron Bing