Hi Team,
he TS pin of BQ24040 uses NTC, and the NTC PAD is laid out on the PCB. The current NTC selection is "NCP15XH103F03RC", and a specification sheet is attached.
1. The current test found that when the temperature is between 40 degrees and 45 degrees, it is thermally protected and cannot be charged, and the battery is not overheated at this time. (NTC mainly detects the temperature of the shell space)
2. Under the condition that the low temperature conditions of BQ24040 remain unchanged, can you recommend a NTC thermal protection temperature higher, such as 60 degrees-65 degrees.
3. The PCB layout and SCH are as follows: