This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: LM5116 compensation calculate

Part Number: LM5116


Hi team,

I need some help to complete the compensation calculation. 

Vin=12V

Vo= -55V

Io= -1.4A

L=22uH

C=220uF(ESR@100mR)