Dear Sir/Ms.
It is stated in the specification that LM74500 can pass the ISO76730 pulse 1 test. For the 12V system, the input load is 12V/2.5A~3A. The waveform of the test is as shown in the figure below.
The customer's terminal product is the headlight of the car, and he hopes that the lights will not flash or flash during the test. Stop. Can LM74500 pass the following waveform test?
Best Regards,
Kami Huang