Part Number: LMR33630
Hi,
I would highly appreciate your help on the issue we have with step-down converter we designed based on LMR33630CDDAR chip. The design is realized according to TI recommendations including component selection and PCB layout. The schematic and layout are below.
We have developed a device with integrated LMR33630CDDAR based step-down converter. It is supplied from 24V big battery that also supplies other electronics. The whole device is consuming up to 2W, so it should not be overloaded. 95 devices are currently installed at our customer and it is working every day for the last 8 months without any problems, except that in the last few months three of them burned. Once we examined those three we realized that built-in fuse burned. When we shorted the fuse in order to check if it is operational, LMR33630CDDAR burned with lot of smoke and light, like a shiny star.
Can you please check the design shared below and share your opinion what could cause this issue. There is always the option that some external distress caused LMR33630CDDAR to burn out, but I am not sure about that since other electronics would burn too.
Schematic:

Layout Top and Bottom layer (two layers PCB, all components are in top layer):
BOM:
| Designator | Value | Package | Manufacture Number |
| R1, R2 | 100K; 1% | 0603 | RC0603FR-07100KL |
| R3 | 24K9; 1% | 0603 |
CR0603-FX-2492ELF |
| C0 | 100uF; V>=50V; Electrolit | EMZR500ADA101MF80G | |
| C1 | 0.1uF; X7R; V>=25V | 0603 | 06033C104KAT2A |
| C2 | 1uF; X7R; V>=25V | 0603 | C0603C105K3RACTU |
| C3, C4 | 4.7uF; X5R; V>=50V | 0805 | C2012X5R1H475K125AB |
| C5 | NOT POPULATED | 0603 | |
| C6, C7, C8, C9 | 22uF; X5R; V>=25V | 1210 | C1210C226K3PACTU |
| C12 | 0.22uF; X7R; V>=50V | 0603 | C1608X7R1H224K080AB |
| U1 | LMR33630CDDAR | LMR33630CDDAR | |
| D4 | Schotky; 1.5A; 40V; 0.54V | MBRS1540T3G | |
| F1 | 50V; 1.5A | 1206 | 044001.5WR |
| L1 | 1.5uH; 27A; 2.5mOhm | 7443330150 |
Looking forward to your reply.