This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A29: TPS548A29 sense pairs

Part Number: TPS548A29

Hi Sir,

When I use the differential remote sense function, can I use 8 mil power trace/8mil gnd trace and the differential length how many mils limitation ?

Is the kelvin sensing to put 0.1uF capacitance between power trace and gnd trace near TPS548A29 ?

If I don't want to use differential remote sense, can I use which value of Rfb_hs from  FB to VSNS- and add 0.1uF from FB to VSNS- ?

  • We will discuss then reply you by early next week.

  • Hi Kevin,

    1. As mentioned in the datasheet, " The connections from the FB voltage divider resistors to the remote location should be a pair of PCB traces with at least 12-mil trace width".

    2. It should be put near the sensing point. Below is a capture of EVM.

    3. If not using remote sense, you can use 10kohm RFB_LS as the resistor between FB and VSNS- and you can calculate the corresponding RFB_HS according to your required output voltage. I recommend not to add any capacitor between FB and VSNS- parallel with the RFB_LS, that would inject a pole in the loop. In most of the cases, that would cause worse load transient performance and less phase margin. 

    Besides, we have calculator tool and Webench tool on Ti.com: https://www.ti.com/product/TPS548A29. Calculator tool is in "Design tools & simulation". You can use them to help with your design.

    Thanks,

    Andrew