Other Parts Discussed in Thread: EV2400, , BQ40Z50
Hello,
I have a problem with BQ28Z610
These are my operations :
1- Power On and activate BQ28Z610, connected to EV2400 (I2C line)
2- The device does not reply to any command (of Battery Management Studio 1.3.101), but I can only download firmware.
3- Once that firmware has been downloaded, everything seems work fine.
4- Power off the device (disconnect the cells).
5- Power On and active the device, but BQ28Z610 return in condition 2, so the firmware not working.
Every information and settings of downloaded firmware disapperar.
Any suggestion? I tried on an identical board, but with IC with different lot and the behavior is correct.
working lot: 94LF,11TO
not working lot: 47LF