This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: can TPS65941212RWERQ1 use same PCB with TPS65941213RWERQ1?

Part Number: TPS6594-Q1

if  i use TPS65941213RWERQ1 in my schematics ,but the IC in my hand is TPS65941212RWERQ1,what should i do?just change TI_NVM_ID ?

thanks!

best regards!

  • Hello Jack,

    The two devices are not drop in replacements for each other. While they share the same power mapping for the bucks and LDOs, the GPIOs are mapped differently and FB_B3 monitors the VDD_MCUIO_3V3 rail in it's corresponding PDN.

    If you are willing to do some modifications to your PCB, you can map the GPIO and FB_B3 using some bluewire connections.

    GPIOs 3, 7, and 9 are the primary ones that need to be changed.