This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61288: Phase compensation design

Part Number: TPS61288


Hello,

I am designing phase compensation for the TPS61288 device.
I calculated Rc, Cc, Cp using equations 12,13,14 in the datasheet.
Attach my calculated Excel sheet.
Rc: 648kΩ, Cc: 440pF, Cp: 218pF (VIN = 4.5V)
The GEA value was obtained from the thread below.

However, when I checked with WEBENCH under the same conditions, there is a big difference between my calculation result and WEBENCH calculation result.
The calculation result of WEBENCH is attached.
Rc: 26.7kΩ, Cc: 33nF, Cp: 82pF

What is the difference between the two?

e2e.ti.com/.../tps61288-calculation-of-rc-in-phase-compensation

Best regards,

TPS61288 calculation.xlsx

WEBENCH TPS61288 5V to12V2A.PDF