Other Parts Discussed in Thread: BQ24610, TPA3220
Dear Sir/Madam,
We have designed the SCH according to BQ24610/LM5121 datasheet and LM5121 online simulation parameters.
Pls help review our SCH design.
The background is as below:
1. LM5121 input is either from switching mode PSU which is 24V or battery pack (15V-18.5V), output 26V/10A to 3pcs amplifiers TPA3220:
1pcs for tweeter, 2x10Wrms, 17.5Wpeak 1% THD @ 16ohm;
1pcs for mid-range speaker, 2x15Wrms, 35Wpeak 1% THD @ 8ohm;
1pcs for subwoofer, 80Wrms, 120Wpeak 1% THD, 160Wpeak 10% THD @ 2 ohm;
2. BQ24610: charge a 5S2P 18650 battery pack (15V-18.5V) via PSU 24V. The battery pack uses BQ78350DBTR-R1 and BQ7692003PWR.