Other Parts Discussed in Thread: TPS62740,
Hello TI team,
We are developing low power (Battery oriented ) device using MSP430 MCU. as earlier Discussion with TI team we shifted from TPS62740 (BUCK Converter) https://www.ti.com/product/TPS62740 to
TPS7A0225PDBVR (LDO) https://www.ti.com/product/TPS7A02#design-tools-simulation
These are our Values
V(In)=3.5V
V(Out)=2.5V
I(Out)=up to 200mA
I(q) would be better if it is nA
After Implementing new design (LDO) to our Device it is observed that our device starts consuming more Current than that of earlier DC-DC converter.
DC-DC used to consume up to 2.5-3mA during normal conditions.
while New LDO is consuming more than 6mA in normal condition
I have attached our LDO schematic here.
Regards,
Vinayak