This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51116: DDR PMIC schematic design review please.

Part Number: TPS51116
Other Parts Discussed in Thread: CSD87355Q5D

TPS5116.pdf

Hi.

I designed the DDR power supply with TPS51116.

FET used BSC0921NDIATMA1, cross reference with TI's CSD87355Q5D product.

I used a small inductor because I didn't have a lot of space on the board.

I used ASPIAIG-F4020-R22M-T and have the following specifications.

ASPIAIG-F4020-R22M-T
Inductance: 220nH
TOL: 20%
CURR: 16.8A
CURR-SAT: 18.8A
DCR: 4.6mR

I wonder if there will be any problems when the circuit is configured like this.

For example, CAP capacity or frequency setting

Then, please check what is possible.

Best regards

KYU