This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54327: Review power supplies

Part Number: TPS54327


Hi,

Attached PDF schematic, please do a review on the power supply and power sequence.

AudioCodes_Power_24.10.2021.pdf

L7= INDC Power Shielded 4.7uH 5.1A 44.1mOhm DCR 4.1X4.1mm

L8= INDC Power Shielded 2.2uH 5.2A 26mOhm DCR 4.1x4.1mm

L9= INDC Power Shielded 4.7uH 5.1A 44.1mOhm DCR 4.1X4.1mm

Capacitors 22uF= CAP CER 22uF 25V 10% X5R 1210.