This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
About the use of LMM IC TPS92662A-Q1, if there is a normal continuous 300mA current through all the LED switch MOSFETs inside the chip (via Drain & Source, DS on), will it have any effect on the chip or this working condition? Are there any potential risks that need to be assessed?
Thanks!
BR
Jiawei
Jiawei,
The TPS92662A is a gated device. I will close this thread and respond to you via email.
-JP