This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: Stop Switching of the DRV pin while avoiding a "Start up/reset loop"

Part Number: UCC28740

There have previously been threads about disabling the switching of the DRV pin however all of the options recommended creating a fake fault (over voltage, over current, etc) )which results "reset loop". This is undesirable for my application: 

1. I want the controller to start switching immediately after I "enable" it.

2. I don't want to waste any unnecessary energy (charge and discharge the Vdd cap). 

I was thinking of pulling the CS pin to an intermediate level ~ around 1V so that I am above the maximum threshold and every switching cycle I won't DRV the primary FET yet I will be below the OVCP so the controller won't discharge the Vdd capacitor. 

Do you think this will work well? Anything I might be missing? 

I can't test  on my own yet, since I am awaiting the EVM..