Other Parts Discussed in Thread: LMR14030
Hi TI experts,
Application is AVN. We need carplay spec for iphone.
1. Is the USB data switch inside the TPS254900 always on after the handshake?
2. If connect the IPHON 12 series, which is less than 20% of the battery, it is charged, but the data connection is disconnected. (Failed carplay)
We are guessing that IPHONE disconnects the data line for fast charging.
But when the TPS254900 is removed and the main to IPHONE direct connected, charging and Carplay connections are possible.
Is there a case that the TPS254900 disconnects the data line?
Please let me know your opinion on this symptom.
It is described in the attached Excel file using the picture and block diagram.
3. Can I get the latest TPS254900 compatibility test report?
Thank you.