Other Parts Discussed in Thread: TPS53314
Hello,
Is the TPS53315RGFR just a 12A version of the TPS53314RGFR? Are there any additional notable features/concerns of using the TPS53315RGFR?
Thank you,
Kyle
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You might have to change the value of RTrip.
|
|
TPS53315 |
TPS53314 |
|
VTrip MAX (V) |
1.2 |
0.6 (Affects current limit threshold as a result. Current limits are lower on TPS53314) |
|
MOSFET resistance (mOhm) |
19 and 7 |
20 and 7.5 |
Thanks,
Caleb