This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563231: burned-out(Vout and SW)

Part Number: TPS563231


Dear team

The product of TPS563231DRLR (VR4) has been burnt out recently.

The burned-out place is the Pin1 (Vout) and Pin2(SW), please refer to the figure below. Could you help to review the schematic and layout?

RT5010W-D187-RoHS-REV3.5.-0807-t.ziprt5010w-d187_power.pdf

Under what conditions, is there a chance to cause this phenomenon!!

If you need more information from the issue, please kindly suggest me.

Many thanks

Denny

  • Hi Denny

    Which software do you used to open the layout? I cannot open it. If it is possible, would you please share the short screen of the layout?

    I would like some extra info. here:

    1. would you please do me a favor to capture the waveform of Vin, SW, iL and Vout when it burnt out? And Vin, Vboot, iL and Vout in the same wavform.

    2.How many pcs out of total had this issue? 

    3.Would you please do me a favor to take a photo of the broken IC?

    The value of the output cap is a little bit small considering the derating. Thanks.

    BR

    Ruby

  • Hi Ruby

    The software tool is PADS.

    1. would you please do me a favor to capture the waveform of Vin, SW, iL and Vout when it burnt out? And Vin, Vboot, iL and Vout in the same wavform.

    => The ic can't work,

    Vin to ground impedance: 17 ohm
    Vout: CP283 impedance to ground: 6 ohm

    Top layer

    Bottom layer

    For layout, Could you help to provide some suggestions?

    2.How many pcs out of total had this issue? 

    fail 20pcs / total 400k pcs 

    3.Would you please do me a favor to take a photo of the broken IC?

    Many thanks

    Denny

  • Hi Denny

    It looks good. Would you please do me a favor to capture the waveform of Vin, SW, iL and Vout of the normal IC? And Vin, Vboot, iL and Vout in the same waveform. The info is limited for me to find the root cause.

    BR

    Ruby

  • Hi Ruby

    Could you have any suggestions on schematic and layout?

    I have capture the waveform of VDS of high side and low side mos. 

    VDS of high side

    VDS of low side

    Many thanks

    Denny

  • Hi Denny

    Here are my comments:

    For the schematic,

    1. The input cap's voltage tolerance is only 16V but with 12V input, the derating will be large. Also, the output cap's voltage tolerance is a little bit low for 3.3V Vout. So I would recommend to use caps with higher voltage tolerance for both input and output, or add one 22uF cap for the input and another 22uF for the output.

    2. I would recommend to add RC snubber to the SW pin to reduce the ring.

    For the layout:

    Just one tiny thing, I would recommend to move the inductor higher, so that the area of the copper for SW can be reduced a little because it is noisy. And then, enlarge the copper for Vin. Others look good.

    BR

    Ruby

  • Hi Denny

    See the layout below.

    BR

    Ruby