This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36520: IBB UVLO

Part Number: LMR36520


Hi All,

is it possible to add UVLO on IBB only with two resistors ? ( we don't need to drive the EN pin form MCU)

Vin=24V

Vout=-9V

UVLO 11.25V (no hysteresis needed)

Br,

D.