This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot run webench simulation for LMR14006Y for wide input range (7.6-30V) and low output current (3.3V/50mA or 5V/130mA)

Hello,

I would like to run a simulation for LMR14006Y for an input voltage of 7.6-30V, Vout =3.3V/50mA or Vout=5V/130mA, but I cannot simulate as I get the following error:

Please change your inputs or select another device.

 

Input data are:
Input:
DC 7.6 V - 30 V
Output:
3.3 V at 0.05 A
Temp:
30 °C

The same error appears also for 5V/0.4A output, which I simulated before

Do you have any advice for simulation/design?