Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G38DBVR.
Please refer to the below image.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G38DBVR.
Please refer to the below image.
Hi, Anusha,
Please see this app note: https://www.ti.com/lit/an/spraby1a/spraby1a.pdf
Best regards,
Don
Thanks Don,
Is this graph applicable for UCC21225ANPLR? i.e maximum reflow temperature =260°C and the time associated with it is 30seconds?
Hi, Anusha,
Table 2 in the document I referenced above has the details you are looking for.
Best regards,
Don