This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24130: SuperCap: different charger current manner using different batch

Part Number: BQ24130


Hi, 

       My customer is CM for big e-meter company. they used BQ24130 for super cap and MP with a lot of this device.  but recently, they found a few of new batch devices show different charging manner as below show.

as can see, the blue one customer think it's abnormal.  the charging current first reach to a high level, then drop to the charging current they set, but normal one, the current ramp up from a level to their setting. 

they confirmed the super cap has been discharging to zero before the test. they want to know what may be the issue. thanks.  

 

        

  • Hello,

    Can you please send a more clear plot that details the current levels at the beginning? This will help me in my analysis.

    Thanks,

    Mike Emanuel

  • please see below picture.  Customer mainly concern about the different charge current manner. 

    do you think if it's normal.  they do did AABB switch. the symptom follow device. 

  • BTW, can you show me a typical charge carve of supercap?  

    1. from their schematic, the charging current should be 320mA, but it shows 210mA, do you think it's normal?

    2.  also , the charging voltage is 11.9V,  according to the settings, I think it should be less than 8.4V( unclear description in datasheet)?

  • NG board 和OK board Data.xlsx

    Attached is their AABB test data and the data source of the pilot.  

  • Hello,

    Please see "Battery Voltage Regulation" in the datasheet. "Internally, the BAT pin has 717 kΩ to AGND. For output voltage above 4.2 V, but not 8.4 V or 12 V, the user can use an external resistor divider from output to VBAT pin to AGND." This means that the BAT pin is regulated to 4.2 V when you connect the CELL pin to AGND. You then parallel the internal 717 kOhm resistor with your external 68 kOhm resistor for a 62.1 kOhm bottom resistor. Regulating 4.2 V at the BAT pin, this makes the output voltage 11.97 V.

    Also, with CMOD grounded, ISET2 determines the charge current. Your ISET2 current is 252 mA. For a sense voltage of 2.5 mA, I would expect the charge current to be in the range of +/-25% to +/-40% according to the datasheet. Even for the best case, +/-25% puts the charge current range from 189 mA to 316 mA. How are other devices comparing?

    Attached is a charge current profile I captured using a Keithley Bi-Directional Power Supply.

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.