This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I drive the UCC27611 GaN Gate Driver's IN+ pin with a 12 volt output from a UC1843 PWM controller? I would connect the UCC27611 IN- pin to GND when doing this.
The UCC27611 mentions that the its IN+,IN- low and high input thresholds are 1.1 volts and 2.05 volts, respectively. The data sheet also mentions that the absolute maximum voltage on those pins is 18 volts.
Regards,
Ken Aquino
Hi, Ken,
Yes, as long as you are running the UCC27611 VDD from at least 12V.
best regards,
Don