This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
1. as below the figure, about θJA and θJC, does θJA =129.5°C/W, θJC=103.9°C/W represent the value of IC monomer?
2. for general test IC on board thermal simulation, should bring in the θJA and θJC value of JEDEC or the θJA and θJC values of EVM?
Hi Tommy,
Thanks for coming to us with your queries.
Kindly see my response as highlighted in blue. For further details on IC thermal resistance metrics, please refer to the attached app note.
1. as below the figure, about θJA and θJC, does θJA =129.5°C/W, θJC=103.9°C/W represent the value of IC monomer? --> Both thermal resistance parameters are based on the Jedec standard.
2. for general test IC on board thermal simulation, should bring in the θJA and θJC value of JEDEC or the θJA and θJC values of EVM? --> To calculate for junction temperature of the IC without heatsink, use the equation below. You can either use the Jedec or EVM values because the difference is not significant.
where:
Tj: junction temperature
JT: Junction to Top package parameter
Power: IC power dissipation
IC Package thermal metrics.pdf
Best regards,
Excel
Hi Tommy,
Just a soft reminder.
Did my last post addresses your queries?
Best regards,
Excel
Hi Tommy,
If you don't have further questions, I will close this thread. You can re-open it by posting your comments.
Thank you.
Best regards,
Excel