Hello everyone and good afternoon,
I am using the BQ24618 in one of my designs to charge a 6-cell Li-Ion Battery, but I am experiencing some problems with it.
The input/system side of the design seems to work fine. When I connect power, the PG indicator LED is turned on, so ~PG is low, indicating good power supply. I can also power the system via the two high-side back-to-back However as soon as I connect the battery, the IC itself releases smoke and gets destroyed immediately, even with no power supply or no system load connected. This is the second board where this happens and I have carefully checked all of the connections for shorts or open circuits, so I can rule out a soldering error and am confident the PCB is manufactured correctly according to the schematic.
I have attached an image of the schematic.
Is there any obvious mismatch with the datasheet that I overlooked? Does anybody have a clue where this error might originate?
Thank you very much and best regards,
Joel