Other Parts Discussed in Thread: LM5118
Hello Team,
I am using LM5118-Q1
Having following load requirements
Input Voltage Range: 6V to 32V
Output Voltage : 5V ± 3% tol
Expected Load current: 1.5Amps
Regulator meets above requirement when switching frequency set as ~307 to 312kHz.
But when I change switching frequency to ~460 to 470kHz the regulator could provide regulation in buck mode till 8V input (decreasing input voltage from 32V) as I decrease input voltage further below 8V the transition from buck to buck-boost mode is not happening (buck-boost MOSFET is not getting gate pulse) & its loosing the regulation. (output going <3V and later getting turned OFF)
NOTE: I can not change switching frequency back to 307kHz or so. I need to have solution for load mentioned above with ~460 to 470kHz frequency only.