This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63000: Iq current is very high

Part Number: TPS63000


Hi,

We are using TPS63000IDRCRQ1 in one of our design.

we are supplying power to this part via  a 3V battery and it is taking 4 mA at no Load.

This Part is taking 160uA current when no load is applied and En pin pull to low.

according to datasheet these values should be very low 50uA and 1uA respectively.

 

Please let me know what can went wrong with it as it is taking that much current.

Note: I have checked each component on  the board and none of the component is draining this current.