This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer would like to confirm with you if we connect DC-48V non standard PoE(50W+) into the PD circuit of TPS23730? Will both TPH and TPL at logic high or low? Customer has tried it and the TPH/TPL will active high. Does it make sense for you, too? Thanks.
Hey Ben,
Is this an adapter voltage? Is it connected to APD? Or is this like a PoE injector on the RJ45 input?
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments
Hi Michael,
Thanks. Please refer the below feedback.
Is this an adapter voltage? Is it connected to APD? Or is this like a PoE injector on the RJ45 input?
There are no adaptor voltage and APD isn't used. They use shottcky diode to do redundant power. Yes, it is like POE injector(non standard) connected to RJ45.
Hey Ben,
Oh okay I understand, then yes this is expected behavior. The TPH and TPL signals are active low. They will only activate according to table 8.2 in the datasheet. The TPH and TPL signals indicate the Type of PSE detected, called mutual identification. However, since the POE injector is simply applying power, the TPH/TPL signals should be high, or inactive.
Does this make sense and is this what the customer sees?
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments