Dear Sir,
I'm trying to select the Current Sense Resistor Rsense for my design.
E.g. Battery is 12V24Ah. Continuous Discharge Current is 20A & Charge Current 12A. Now I want to set the Over Current Discharge protection at 25A & Over Current Charging Protection at 15A.
bq7791506 OCD 1 Threshold is 50mV, OCD 2 Threshold is 100mV, OCC Threshold is 60mV & SCD Threshold is 300mV.
- For discharge protection which OCD threshold to consider to calculate the Rsense? OCD 1 or OCD 2?
OCD 1 = 50mV then, Rsense = 50/25 = 2mohm,
OCD 2 = 100mV then, Rsense = 100/25 = 4mohm,
OCC = 60mV then, Rsense = 60/15 = 4mohm
SCD = 300mv then, ISCD = 300/4 = 75A & 300/2 = 150A.
- Which Rsense value to select so that both charging & discharging protections will be achieved?
- Can you please explain one more calculation using any random current value?
Regards,
Samruddhi