Other Parts Discussed in Thread: LP8866-Q1
I have a question on boost switching frequency selections on LP8866S-Q1. Below shows the Fsw options listed on the data sheet. I want to know if these 8 frequencies are the only options, or if it's possible to achieve another frequency in-between using a different BST_FSET resistor value. For example, could we configure 600kHz if we use a resistor value between 11kohm and 17.8kohm? Thanks in advance.