This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Good day! I'm posting this on behalf of the customer.
Here it is:
I am using your BQ24080DRCR to charge a 4.2V lipo battery. I want to charge the battery iven if it is connecter with the opposite polarity.
I see this circuit:
Three questions:
1) will this circuit work with the BQ?
2) what happen with the BQ (with this circuit) when i unplug the battery?
3) what happen with the BQ ( with this circuit) when i unplug the USB ?
Also, what happens with the BQ when i unplug the battery with this protection circuit?
Best regards,
Jonathan
Hi Jonathan,
I want to charge the battery iven if it is connecter with the opposite polarity.
This is an interesting request, just so I understand:
Normal polarity: Q2 / Q3 ON, Q1 / Q4 OFF
Reverse polarity: Q1 / Q4 ON, Q2 / Q3 OFF
The BQ acts like a current source up to the battery regulation voltage, should be able to simulate the circuit to see if it works. May also want to add series resistance to the gates to avoid ringing.
It is possible to add reverse polarity protection, we have circuits for this you can refer to here: https://www.ti.com/lit/an/slva139/slva139.pdf
Best regards,
Nick
Hi Nick,
Thank you for your support and sharing important details. I will update you once our customer have a follow up question.
Best regards,
Jonathan.
Hi Nick,
Here is our customer's update.
1
It looks like this may work, you would still want to have primary protection for the battery to prevent undervoltage, overcurrent etc..
-I thought the BQ has all those features right?
2.
It is possible to add reverse polarity protection, we have circuits for this you can refer to here: https://www.ti.com/lit/an/slva139/slva139.pdf
- In the document that you shared it seems to show a passive load (not a battery charger) if I use a battery charger I suppose that in have to connect the MOSFETs with the diodes pointing the load right?
Best regards,
Jonathan
Hi Jonathan,
Cell under voltage and over current protection is not possible due to bq24080 being non-powerpath, the system load is connected in parallel with the cells. A power path charger can include these features check out the BQ25180 (Buvlo, BATOCP).
TI offers primary protectors such as this one: https://www.ti.com/product/BQ2970
- In the document that you shared it seems to show a passive load (not a battery charger) if I use a battery charger I suppose that in have to connect the MOSFETs with the diodes pointing the load right?
No changes are needed to the circuits in figure 2/3.. here is a drawing with charger included:
Best regards,
Nick
1) will this circuit work with the BQ?
It may work -- but worst case is that somehow a FET fails and you short BAT positive to BAT negative. Without any primary protection for the cells this would be a very fiery failure for the battery.