Other Parts Discussed in Thread: LM3488, LM7480-Q1, LM3478
Hello,
I have a strange issue with LM3488 that happens only when my design has connected load. (> 0.5Amp) during startup.
Input is 12V and configured output is 24V.
Seems that the LM3488 is locked at 50KHz (I measure 50KHz on FA/SYNC/SD pin) and N-Mosfet exhausts all available current of the power supply. (In my test case I have limited current to 5Amps)
If the circuit is connected to power without load or load below 0.5Amp, it works as expected during startup. Measured frequency is 350KHz during normal operation.
Thank you for your help.