This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: Battery RSOC / SOH jump at the -10℃ (battery have GPCRB )

Part Number: BQ28Z610
Other Parts Discussed in Thread: GPCRB

Hi team,

Here's an issue from the customer may need your help:

When encountering abnormal conditions in practical application, Voltage V.S RSOC has a big drop and they also see the SOH is float.
(EX: @-10℃ the Voltage=4.2V to 3.6V, RSOC=100% to 1%, SOH=100% to 25% )


The same question was asked before, and they try to use the GPCRB method to correct

The reference URL is as follows:
e2echina.ti.com/.../bq27542-g1-at-0deg-charging-jump-soc-12-to-0

Pack information:
CELL NCR18650BD 1S3P , GG chemistry ID 2072
Test conditions : @ -10℃ discharge 440mA / 30sec & relax 60sec, cut off SOC=0% or Voltage <3.0V

2022-01-27_01-RMA_ DISCHARGE.log.rar0576.gg file.rar

Could you help check this case? Thanks.

Best Regards,

Cherry