This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
If you have 3 outputs in LM5180 application all with low power, is there any data about control and cross-regulation?
How do I force WebBench to optimize with this particular controller?
An important issue: a lot of such chips are "no-stock" ...any suggestion of using those that are in stock?
How do I locate such chips?
Any help will be high;y appreciated.
r
Hi, Robin,
If you want 3 output simulation in webench, please set Iout to 3*50mA as my example 150mA send to you.
then if need to check single out performance, sent to 50mA should be work.
Webench could custom design a transform or change to other value , please click the component on SCH, example as below. choose alternate then input the value in your design to do simulation.
Wish it could help you.
Elena
Robin,
For "no-stock" ..device , only way is to change a part with close spec. Or you could connect your local marketing or sales to check if they can support sample.
Elena