This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TPS544B20 data sheet provides current sense accuracy for load currents between 3A and 20A. What happens to the accuracy below 3A?
Customer is seeing wide variation from unit-to-unit with load around 1.5A with readings from 0 to 3A. This is within the +/- 3A spec listed for loads above 3A, but I would expect the current sense amplifier gain error to be small at low currents. Could the offset error be this high, or do other error sources come into play below 3A?
The vast majority of the ±3A tolerance on the reporting error is offset error not gain error. Of the ±3A range, about 2A is offset error and 1A is gain error over the 3A to 20A range.
The current sense and reporting, pre-averaging, is also clipped at 0A, so it can not measure or report negative currents.