This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Reference Experts,
for TL431LI in the DS the continuous cathode current is specified with a max value of 18mA.
Do we have some data for short term load ?
My customer is looking into short loads up to 21mA for ~1ms.
Normal continuous operation is at
Can the part withstand the 21mA for 1ms ?
Many Thanks
Best wishes,
Olrik
Hello Olrik,
This is above the abs max rating of the device and not recommend. Thanks.