Hello,
My name is Abhishek K SIngh and I was using UCC21521 to provide gate signal to a Hex-bridge to control position of a BLDC motor. I have used three UCC21521 ICs, one to control one leg (high side MOSFET and Low side MOSFET) in the Hex-bridge. I'm using a bootstrap circuit along with UCC21521.
I was testing this motor with a spring load. There was some displacement command given to motor after which command was givcen so that it can come back to its natural position (when spring load is 0Nm).
While coming back to its natural position the MCB (16 A rated) put for protection of 150V motor battery power supply tripped. It was not know what has happened in the ECU so, MCB was swutched ON again but it tripped again, and there was a sound heard from the ECU. When we opened the ECU what we observed were as follows:
1) Capacitor C102 burnt and blown up along
2) Current sensor U20 pin 3 & 4 to 150V PB_GND (150V power ground) track burnt and evaporated
3) MOSFETs Q2 and Q5 were showing short between Source - drain, source - gate and drain - gate.
4) MOSFET Gate drivers U1, U2 and U3 ( not shown in circuit but it controls third leg of Hex bridge) were damaged:
a) OUTB - VSSB short was observed in all of them
b) VDDB - VSSB short was observed in all of them
c) OUTA - VSSA were not shorted
5) Output side of 28V to 15V DC-DC converter powering all the MOSFET gate drivers was shorted.
Schematics: UCC21521 ckt.pdf
I'm current in the process of root couse analysis for this failure and was to know what kind of electrical stress could cause the MOSFET gate drivers to fail in the way they have. Please help me regarding this.
I would also appreciate if you had any recommendation regarding the circuit,
Regards,
Abhsihek Kumar Singh