This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
We will use LM7481-Q1 with a redundant supply design. Whether two LM7481-Q1 DGATE interactive switches when VIN1=VIN2? If yes, does it make any side-effect?
Regards,
Hsing
Hi Hsing,
When 2xLM74800-Q1 are used in ORing configuration, the DGATE of LM7480x-Q1 with highest value of (Input Voltage - Load current x Path Impedance) would be ON. A small difference of this voltage (4.5 mV) between the two supplies can cause one of the LM7480x-Q1 to turn OFF its DGATE.
As you mentioned if there is case where the VIN1=VIN2 and path impedances Z1 = Z2 , then the DGATE's of both the LM7480x-Q1 would be ON. Then the load current would be equally shared between each path. There would be no problem if both the DGATE's are ON.