This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73801-SEP: /EN pin low level?

Part Number: TPS73801-SEP

Hi,

In the Revision A (May 2021) datasheet, two values are specified for worst-case low level for the /EN input pin - in chapter 6.3 (recommended operating conditions) it is 0.25V - in chapter 6.5 (electrical characteristics) it is 0.15V.  Just a typo, and if yes then what is the correct value - or is there more to it than that?

Cheers, Martin

  • Martin,

    Thank you for pointing this discrepancy out.

    The 0.15 is the correct VIL max value to insure device is disabled.

    I will have the datasheet updated to remove the errors.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade